Part Number: TLV3603
我想用TLV3603比较器,输入一端是一个正或者负2V的信号,另一端是地信号(作为0V),通过比较这两个信号,来实现比较器的翻转,不知道在这种应用的情况下,VCC接+2.5V,Vee接-2.5V,并且配置LEHY管脚来实现hysterisis,是否可以实现我的功能?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我先按照单电源供电,1/2VCC=2/5V 为参考,加了30mV迟滞,是可以的:

但是如果改成+-2.5V供电,+-2V输入,GND作为参考,30mV迟滞,输出恒为高:

您好,我看了下TLV3603的数据手册,2.7V和5.5单电源范围,因此是可以+-1.35V~+-2.75V双电源范围,并且这颗比较器是轨至轨输入输出的,所以在+-2.5V供电条件下,参考电压为GND,输入+-2V都是满足输入电压要求的,也就是说VEE是允许负压供电的。

我上述按照双电源供电仿真结果一直为高,理论上是不对的,所以我要确认下是不是model这里的VEE只能接GND,因为我进入Macro库文件之后看到VEE是这样描述的:
In some simualtors (Cadence), it may be necessary to add a 1 micro-Ohm (1u) resistor in series with VEE to circuit GND (0 node) for proper operation。
您好,按照我上面的描述,TLV3603的VEE是可以-2.5V供电的,并且输入+-2V和0V作为参考都是满足其输入电压范围的,所以这样应用是没问题的。
TINA仿真一直为高,我去确认了下,是model的问题。