使用OPA828搭建带缓冲的Howland电流源(图1所示),电路板在功能上得以实现,IN端输入1Hz~100kHz的正弦波,OUT端可输出1Hz~100kHz频率范围内的正弦电流(电流幅值由输入信号幅值与电阻R3确定),但在高频大负载条件时,实际输出电流明显衰减(eg:设置输出电流8uA,频率100kHz,负载为100kΩ,但实际负载上电流只为5uA甚至更少,且负载越大或频率越大,衰减越严重),请问如何解决高频大负载条件下输出电流衰减的问题.
图1
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您的意思是采样电阻R3是10K,其他电阻是20K?建议将电阻调小以降低热噪声。电路中的大电阻和寄生电容可能导致的带宽限制和稳定性问题。
下面参考设计中设计步骤您可以参考:
下面文档希望对您也有帮助: