Part Number: INA293
INA293A4IDBVR at 45℃ and 85%RH . The output voltage was 1.05V to 1.5V, as shown in the figure below. At this time, the input signal(pin 3-pin 4) was 0mV. The output voltage was 0V after being left at room temperature. Please help analyze what is causing this.