This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA281: 请问PGA281支持全差分输入,全差分输出吗?

Part Number: PGA281


我的输入是一个全差分信号(正负10V),输出我要正负2.5V的差分信号,我用PGA281合适吗?

  • 您好,可以的,PGA281是差分输入差分输出,所以是一个全差分的可编程增益放大器。

    我的输入是一个全差分信号(正负10V),输出我要正负2.5V的差分信号

    由于不是轨至轨输入,所以在输入+-10V时,要注意电源电压的范围,可以看到供电电压的范围至少在-12.5V~12.5V范围才能保证+-10V输入, 因此可以直接使用+-15V供电。