This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM318: LM318

Part Number: LM318

 如图,将LM318用作差分放大,供电为5V,输入悬空或将输入同相段与反相端短接,在输出会有1.3V输出,为什么

  • 您好,

    LM318 最小供电电压为±5V(或单电源10V),使用单电源5V供电不满足规格要求:

    像运放这样的模拟电路一般不允许悬空输入,这可能使输入、输出过载损坏运放。

    另外注意满足运放的输入和输出范围。LM318 不是轨至轨输入和输出运放,在单电源供电时输入和输出范围达不到0V。根据datasheet 如下截图,输入需要距离电源轨3.5V,输出需要距离电源轨3V。

  • 将两输入端短接,Rs电阻相当于对地下拉,采用单电源15V供电依然会出现相同的现象

  • 将两输入端短接,

    那相当于输入为0V,那输出也是0V,如果单电源供电,如上所述,输入和输出都不满足规格范围。

x 出现错误。请重试或与管理员联系。