Other Parts Discussed in Thread: INA190, INA293
请帮推荐个运放:主要参数如下:
共模输入电压: VCM ≥40V
带宽:BW ≥200KHz。
压摆率: SR≥2V/us 以上。
放大倍数:50倍、100倍、200倍。
通道数:单通道,双通道,4通道都可以。
其它:需要有REF 脚。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,由于上次的问题比较久了,为了更好的跟进您的问题。我将您的这个新问题重新建了一个新帖。
您好,您可以看下INA241::Vcm: −5 V to +110 V, SR: 8V/us ,也带有REF参考引脚,但是增益是根据不同的后缀而不同:

同样,INA190,INA293也都能满足要求,都是和INA241相同,不同的尾缀型号实现的增益有差异,因为这些器件都是固定增益的。