Other Parts Discussed in Thread: AFE031
我用AFE031芯片做设计,PA给的16v电源,但是在没有设定任何内部寄存器的条件下,REF1测到电压2.5V,REF2没有测到电压,我用的是资料中44页中的参考设计,还有Tx-FLAG和Rx-FLAGd的电压均小于1V,我的板子的PCB 是自己绘制的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的PA端的电压实际测量时为16V,电阻和电容采用的都是0603的贴片封装,图片中的是原理图,电源都是外部提供的,我焊了两块板子,第一块AFE031底部的焊盘没有焊接上,第二块底部的焊盘接地了。在功放的输出端,第一块测的时候开始是1伏左右,后来没有了,第二块是4.7V左右,但是两块的REF1都是2,5V左右,REF2用万用表测量是几毫伏,这些都是在未设置寄存器的条件下得到的,我觉着不对,还有RX和TX的输出端都测不出电压 。之后连接控制芯片采用的是STM32103ZET6,软件设置后,输出也没有反应
电路是参考设计,所以电路上没有问题。
在确认一下layout, 芯片底部的焊盘必须接GND, 而且要充分的焊接,采用多层板的打孔设计,详细见www.ti.com.cn/.../afe031.pdf 第十四六/十四七页,PowerPad的设计目的就是给芯片散热,如果芯片不散热很容易就造成芯片热保护,不接GND很容易造成芯片不良。PA是主要的功率(热)消耗,PA损坏,REF1肯定会异常。
另外,电路图没有问题,就再确认一下是否有焊接短路。
(layout 参考:www.ti.com.cn/.../sboa130a.pdf)