This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2994: 通道隔离与频率间关系的测试

Part Number: OPA2994


您好,打扰了!

我看到OPA2994中有一张通道隔离和频率间关系的特性图。 请问,如果我需要测试1kHz处器件的通道隔离度,应该如何设计测试电路呢?

期待您的回复!

  • 您好,

    通道隔离就是一个通道对另一个通道的干扰程度,就是串扰,这是多通道放大器的参数。如果在1khz时通道隔离值为120dB,就是一个通道输出信号峰峰值为1V,频率为1KHz时,在其他通道将产生峰峰值为1uV的同频率信号。测量的话就是一个通道输入1KHZ的信号,然后看在另一个通道输出同频率电压产生的幅值,输入信号幅值与另一个通道输出同频率电压幅值的比率就是串扰值。

  • 谢谢您的回复!

    我想问一下,如果是双通道的运放,我将A通道接成跟随器,输入1V,1kHz的正弦波,此时可以测得A通道的输出峰峰值;

    那B通道的输入端也需要接成跟随器,还是直接悬空测此时B通道的输出端电压值?

  • B通道也需要接成跟随器,注意B通道的输入和输出需要在运放线性工作范围内。

    A通道有10kΩ负载: