Other Parts Discussed in Thread: INA228
HI ALL
想请教一个在应用时的问题,我们正在使用INA228产品做一些简易电池检测的应用,由于INA228自身没有防反接设计,我们尝试通过NMOS控制地的通断来实现防反接。但在实际设计中,我们注意到,仅仅将地进行分割是不够的,I2C及VS上也必须通过二极管或体二极管进行隔离。我们理解也可以测到MCU内部的Zener管路径,但不太明白INA228中为什么会有I2C或者VS正向对地的路径。
我们使用万用表二极管档位直接对INA228的I2C和GND之间进行测试,INA228_GND->I2C有一个二极管的压降,这是正常的。反向并没有测到任何压降,但是在连接MCU后,两个地之间便存在1.2V的压降(MCU_GND->INA228_GND)。我们断开了其他所有路径,这个现象仍然存在,结合二极管隔离后的作用,我们推断这个路径来自INA228,但不太理解这其中的原因。
希望能得到你们的解答,感谢!