Part Number: LM2903


The relationship between VICR and temperature,The lower the temperature, is it VCC-2V, or -40 degrees Celsius -2V;Full range 0 to VCC-2 ,What's the temperature range,There is no temperature correlation
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
LM2903全温度范围是–40 ~ 125°C:

其电器特性看6.12章节表格内容:

在25°C时其Vicm 是0 ~VCC-1.5V,在全温度范围内或者说在其他温度Vicm 都是0 ~ VCC-2V,不管是比25°C低的温度还是比25°C高的温度。
其共模输入电压与温度没有明确的对于关系,datasheet 都没有给出。我们在应用时,一般选取最小范围值即其Vicm 是0 ~ VCC-2V。
另外注意所附截图与官网中有所区别,请在TI官网查看最新版的datasheet:
https://www.ti.com/lit/ds/symlink/lm2903.pdf