在XTR117的数据手册www.ti.com/.../xtr117.pdf
第3页,参数SPAN Error,在Io = 200uA to 25mA时,
TYP = 0.05%,MAX = 0.4%。
是否可以理解为TYP误差为12.5uA
MAX误差为100uA。
这个误差比较大,是不是理解错误?
正确的算法应该是怎样的?转换为电流误差为多少?
非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在XTR117的数据手册www.ti.com/.../xtr117.pdf
第3页,参数SPAN Error,在Io = 200uA to 25mA时,
TYP = 0.05%,MAX = 0.4%。
是否可以理解为TYP误差为12.5uA
MAX误差为100uA。
这个误差比较大,是不是理解错误?
正确的算法应该是怎样的?转换为电流误差为多少?
非常感谢!
你好,
SPAN Error指的是增益的误差,在XTR117中,SPAN是100,取MAX Error的情况下,SPAN应该是99.6~100.4。
计入SPAN Error时,取MAX值的情况下,Io = Iin * (99.6~100.4)
在Io预期应该为25mA的时候,Iin应该为250uA,这个时候TYP误差为250uA * (100 * 0.05%) = 12.5uA,MAX误差为250uA * (100 * 0.4%) = 100uA。
在Io预期应该为10mA的时候,Iin应该为100uA,这个时候TYP误差为100uA * (100 * 0.05%) = 5uA,MAX误差为100uA * (100 * 0.4%) = 40uA。