芯片的3.3V的供电正常,但是输出的电平高电平和低电平电压均不对。如下图1所示,方波为比较器的输出信号OUTA,高电平为1V,低电平为0.5V。如图2所示,方波为比较器的输出信号OUTB,高电平为1V,低电平为0V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 1; //ECAP3 GpioCtrlRegs.GPAPUD.bit.GPIO9=1; //禁止上拉使能 GpioCtrlRegs.GPADIR.bit.GPIO9=0; //配置成输入 GpioCtrlRegs.GPAQSEL1.bit.GPIO9 = 2; // 0=>Sync to SysClock; 1=>3*Tsa; 2=>6*Ts GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 1; //ECAP4 GpioCtrlRegs.GPAPUD.bit.GPIO11=1; //禁止上拉使能 GpioCtrlRegs.GPADIR.bit.GPIO11=0; //配置成输入 GpioCtrlRegs.GPAQSEL1.bit.GPIO11 = 2; // 0=>Sync to SysClock; 1=>3*Tsa; 2=>6*Ts
GPIO的配置如下,试过改变GPIO的输入输出、上拉下拉,都不能解决输出电平错误的问题。