Part Number: LM211

上图中电路正常工作时的波形应该是下图这样的,输入是7V以下的负电压波形,黄色的那个是输入波形,蓝色的是比较器的输出。

当去掉原理图中的R62、R63、R64输入电阻后,当电压超出-7V的电压值以后,比较器输出不正确,如下图:

初步判断是比较器输入电压或电流过高导致的输出错误,但具体原因没有分析出来,希望哪位高手能够解答一下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
初步判断是比较器输入电压或电流过高导致的输出错误,
是的。我看您是使用单电源5V供电,可以看到输入信号的电压范围为VCC- +0.5V~VCC+-1.5V,所以5V单电源供电的话,输入信号的电压范围为0.5V~3.5V,超过这个范围会影响比较器输出翻转,导致输出错误。
所以如果您需要-7V以下的输入,那么可以考虑双电源供电,比如+-10V,+-10V供电输入信号的范围在-9.5V~8.5V范围内,保证比较器的正常工作。