This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4189: 微弱直流信号测量方案——增益校准问题。

Part Number: OPA4189


老师们好,我有一个直流增益校准问题请教。

要求:

1.输入信号50nv~5u直流信号。分辨率5nv或者10nv。直流增益500倍。

2.电路中存在噪声、温漂。其中电阻温漂+-5ppm。opa4189温漂5nv。

3.使用复合放大。使用两个运放,第二个运放输出反馈到第一个运放负反馈端。

4.为了提供系统性能或者测量精度。提出了实时动态直流增益校准。

5.放置基准芯片。基准信号通过电阻分压,得到1uv和2u电压。

6.原本想通过这两个电压实现增益测量。1u和2u电压存在温漂、噪声。非常不理想。

7.能否提供一个ti参考方案。实时校准方案,且精度高。

8.还有就是1u和2u方案是否就是错的呢?我还考虑过直接输入无源器件,比如电阻,有可能实现吗?这个方案也麻烦可看看。