Other Parts Discussed in Thread: OPA695
你好,如图所示,R3400左端输入的是1.25v的直流电平,我们使用的是OPA695ID,这样的话6脚的输出理论上为1.25V的电平,但当我将OPA6965ID更换成AD8009时,其他参数不变,则输出6脚为负3.9V,OPA695的3脚不为1.25V,而为负的1.8v,有么有大神能帮我解释一下这个现象吗,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,正向端是接入了一个10K和30K的电阻,5V进行分压,这样会得到一个1.25V的直流电平,在负向的输入端,接入了一个直流电平为1.25V的交流信号,这样VOUT=6*1.25V-5*(1.25V+交流信号)=1.25V-5*交流信号,所以没有超出电源轨,但当这个电路接入AD8009后,正向端的5V分压电路不为1.25V,而为负的1.8V,这样导致电路负向饱和,输出为负的3.96V,这样就没有放大交流信号。在起初的测试中没有接入交流信号,负向端只有1.25V的直流电平,所以理想情况下,输出应该为1.25V的直流电平,谢谢!