Part Number: TLV333
Other Parts Discussed in Thread: OPA333, OPA391, OPA328, OPA928, OPA325, LMP7701, OPA320, OPA392
Hi 支持者,
请教一个问题,TLV333的输入阻抗是多少,我在datasheet中并未看到这个参数。同时再请教一下,opa333的输入阻抗是多大,两者有无对比文档可以分享下。
谢谢您的支持。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
之前也有客户问过类似的问题,TI的答复是
Unfortunately we also do not have any data on the input resistance of these devices (this can actually be a very difficult parameter to measure, especially for low voltage devices). Given that these devices are both made on a CMOS process however, a good estimate for these parameters would be 100MOhms for the differential resistance and 6000GOhm for the common-mode.
原文参考这个链接
关于OPA333的输入阻抗,给的阻抗值可能更加不确切,
Both, CMOS and JFET input op amp may have input impedance in the range of 1Tohm but for the low voltage and RRIO CMOS would be the only choice. Please take a look at OPA328, OPA392, OPA391, OPA320, OPA325, OPA333 for 5V supply or LMP7701 (Vs up to 12V) and OPA928 (Vs up to 36V), etc.
原文参考这个链接