Part Number: OPA211
我在使用OPA211时,+5v单电源供电,输入端接入200mV直流电,,输出端测到400mV左右,disable 运放以后,输出端测到0v,但是如果此时继续增加输入端电压,就会发现输出端还是能测到电压,输入2.5v时测到输出有80mV,另外一个问题是,运放使能的情况下,输入0v,但是输出端会测到50mv的直流,disable之后就测不到了

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,您的描述用的+5v单电源,与提供电路图不符。关于disable, 请注意shuntdown电压范围为(V+) – 0.35~(V+)。 请确保为该电压范围。 如果是单电源,输出电压范围是到不了0V的, 请参见手册Vout范围。同样5V供电,输入是2.5V也会使输出饱和。