Other Parts Discussed in Thread: OP07, OPA2333, OPA333, OPA335, ADS1247, ADS1248
OPA2333比OP07低多少?单电源5伏时,能从0伏开始放大吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主你好,能从0V开始放大的。
Datasheet上写着:
The OPA333 and OPA2333 input common-mode voltage range extends 0.1 V beyond the supply rails. The OPA333 is designed to cover the full range without the troublesome transition region found in some other rail-to-rail amplifiers.
这个运放甚至可以输入略低于0V的电压,而且还可以输出略低于电源轨0V的电压。
昨天RC 输入端电压,和 OPA333 Vo电压比较,竟有15mv压差.万用表不太准是一方面.
很纳闷,将两个100K的电阻换成5k, 再测RC输入端电压,和 OPA333 Vo电压比较, <0.1mv 偏差(4位半表).
至此OPA333工作基本正常,OPA333 Vo经5k电阻接LTC2401 ADC输入,ADC结果仍差10(10*3v/65536=0.458mv)
问题缩小到 OPA333与ADC匹配上。 本来传统ADC 输入采样电容,采一次就行了。sigma-delta ADC 是否要采很多次,
而且要做50/60hz 滤波, OPA333 手册上说自动校零 8us一次,LTC2401输入开关电容切换f=150khz. 这两者会不会有影响?
目前看,ADC结果总差10, 准备直接加10, 不校准了。本来用OPA333就想在校准上省点事。
关于OPA333与SIGMA-DELTA ADC皮配的问题,在网上找到一说法是:压摆率不太高的OP不能与SIGMA-DELTA ADC 直连!
开关采样电容闭合,OP输出闪速拉低,ADC BUFFER OP受压摆限制, 输出给采样电容充电有一上升时间.
最好是OP>>RC>>SIGMA_DELTA ADC . RC除了抗混作用,另外当开关采样电容(2~4PF)接通时, RC中的C还能给采样电容快速充电.
OPA333的datasheet提到, 输出端的Cl, 又不能太大,会增加过冲.
OPA333匹配SAR ADC应没问题, 430也有内置SAR ADC的型号,但没提到有50Hz/60Hz数子滤波功能.
另一方面, 对低功耗设计, MSP430 , OPA333是理想选择. 作设计就是多种因素的权衡折中.
ADS1247/8 功能强大,集成了ADC buffer OP, SIGMA-DELTA ADC, 50Hz/60Hz滤波。
好像在哪儿看ADC buffer OP到类似OPA333。
望TI能提供OPA333与SIGMA-DELTA ADC皮配时的接口设计。
OPA333与LTC2401配合,ADC结果如果恒定少10个字,也没问题。
做产品,也没条件精细测试,小批OK,不知上量是否还恒定少10个字。
再作产品准备换用ADS1248,当时没选主要是想输入动态范围再大些。 现再操心了。