Part Number: OPA192
您好,
有一个项目中用到OPA192这个放大器,有两个问题:
1.V+是+12V供电的,V-是-12V供电的,想问下+12V和-12V这两个电有没有什么必须的上电时序需要控制?
2.还有就是我的项目中是通过FPGA的GPIO管脚来控制OPA192这个放大器的+IN,但是OPA192先上完电,FPGA再上完电,OPA192先上完电会不会有什么漏电流到我的FPGA,影响到我的FPGA?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
1.V+是+12V供电的,V-是-12V供电的,想问下+12V和-12V这两个电有没有什么必须的上电时序需要控制?
建议同时或者尽量接近同时给其供电。
2.还有就是我的项目中是通过FPGA的GPIO管脚来控制OPA192这个放大器的+IN,但是OPA192先上完电,FPGA再上完电,OPA192先上完电会不会有什么漏电流到我的FPGA,影响到我的FPGA?谢谢
如果OPA192的输入在FPGA未上电时处于不确定状态(如浮空),则可能会通过GPIO管脚向FPGA注入电流,尽管这种电流可能很小,但长时间累积或电流过大仍可能对FPGA造成损害。所以OPA192的输入(如+IN)在FPGA未上电时处于高阻态或已正确配置,那么应该就不会有太大的影响。