This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LOG200: 关于替换芯片带宽的问题

Part Number: LOG200


目前我司使用的是AD8305寻求LOG200进行替换,关于LOG200的信息仍然是偏少的,我希望获得更多关于它的信息,主要点是关于带宽的问题,我们的光学系统设计的带宽计算为最高可能达到20MHz,在对数输入部分,我并不清楚如何换算,我知道对数放大器会对带宽进行压缩,LOG200的 LOG_OUPUT_BANDWIDTH是6MHz,我该如何换算它的输入带宽最大范围?同样的对数放大器AD8305写明的是最大值为15MHz的带宽,目前我们系统的性能在不断提升,需要寻求更好性能的芯片,所以我需要获得更多关于LOG200的信息与对数放大器的信息。

请帮助我