This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OP07C: 使用运放实现LED恒流源驱动,输出漂移

Part Number: OP07C

原理图上图所示:

在将pwm输入设置为0的时候,通过调整电位器VR36可以将运放输出调整负电压。所以调光mos Q21是关闭状态。此时led是全部关闭的。

目前遇到的问题是:过段时间,上电后将pwm调0后,运放的输出是还会有2v左右的电压,所以回造成led灯珠是微亮的。但是将led点亮半小时左右。在pwm输入为0时,是可以正常关断,运放输出会是负电压。

所以请教下,这个是因为温度带来的温漂吗?还是说VR36电位器不参数不稳定造成的?

如果是因为温度问题的温漂,请教下这块温漂抑制有合适的修改方案吗?

谢谢~