http://www.ti.com.cn/cn/lit/ds/symlink/ths3091.pdf 里边的TYPICAL ARBITRARY WAVEFORM
GENERATOR OUTPUT DRIVE CIRCUIT
中DA之后的放大电路能用一个放大器解决吗?或者说电压放大器之后的3个电流放大器,可以用一个电流放大器吗?
请推荐:)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
http://www.ti.com.cn/cn/lit/ds/symlink/ths3091.pdf 里边的TYPICAL ARBITRARY WAVEFORM
GENERATOR OUTPUT DRIVE CIRCUIT
中DA之后的放大电路能用一个放大器解决吗?或者说电压放大器之后的3个电流放大器,可以用一个电流放大器吗?
请推荐:)
你好!
需要根据最终的负载来决定。ths3091中的典型应用采用三颗3091并联输出,是为了提高输出功率。
我是想用一颗放大器来达到3颗的效果,同时保证3091中的带宽(50Mhz)大概输出电流是500mA
最好有一个放大器,能够代替所有的放大部分,包含前边的电压放大器。
看看这两篇帖子能否解决你的问题:
“www.deyisupport.com/.../1619.aspx”
“www.deyisupport.com/.../4379.aspx”
感谢您的回答呵呵。我在学习您推荐的这2个文章:)