您好,opa2354能做电压跟随么
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
可以, “The OPA354 series are unity-gain stable and can drive large output currents.”
请参考:
VCM 不影响噪声的前提是VCM和输入输出都在运放的线性范围内,对于50K电阻和100欧电阻的组合来说,这个电压是不正确的,单电源输出摆幅在电源负轨上100mV。
因为输入阻抗在高频情况下的变换,所以OPA2354的电流噪声建模很复杂,实际建模结果与手册不太吻合。建议您使用TLV354来做噪声分析,这两个模型的噪声非常接近。而TLV354的电流噪声与OPA2354手册比较吻合,而且在高频下更加准确。
仿真看附件这个吧,仿真频率要比带宽高些,直到总噪声达到稳定水平。
关于噪声计算可以看一下培训视频: