This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
仪表放大器INA128的输出是相对于管脚REF的电压来说的.即 Vout = Gain*(Vin+ - Vin-)+REF.
REF接电压基准的目的是提高输出的电位。
产品手册上说,一般REF接地,而且要低阻抗相连。
“The output is referred to the output reference (Ref)terminal which is normally grounded. This must be a
low-impedance connection to assure good common-mode rejection. A resistance of 8
Ω in series with the Ref pin will cause a typical device to degrade to approximately 80dB CMR”
下图是一个REF不接地的例子。
运放保证了低阻抗连接。"The op amp buffer provides low impedance at the Ref terminal to preserve good common-mode rejection."
运放保证了低阻抗连接,是不是因为运放的输出电阻比较小?如果我要在INA128的REF管脚接2V的电压基准,是不是也不能直接连接,需要加一个运放?
有些基准的输出阻抗也很低。
一般运放的低频输出阻抗会比较低,如果是高频阻抗需要比较低,最好使用电容来降低阻抗。
我用的基准是REF5020, 算出的输出电阻是0.06欧姆,是不是已经很低了?可以不要运放?