This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有关OPA835作为滤波器使用时遇到的问题求TI得大神帮我解决,万分感谢

Other Parts Discussed in Thread: OPA835

1、最近在利用OPA835设计滤波器电路时,发现焊接出来后遇到几个问题无法解释,实在是找不到原因,求TI的大神帮助!万分感谢

2、在tina仿真时也有电路中部分不是很懂,想请大神帮我解惑,谢谢

3、具体的问题我以附件的形式上传了(详见附件)

 

 

 

4、有关OPA835的相关问题:
根据TI的FilterPro 软件设计的200kHz的滤波器电路如图,主要问题有:
(1) 在利用tina进行仿真时,发现C1、C2、C4、C3不可以去掉,去掉了就没有输出了。我
想知道这是为什么?
(2) 在实际进行焊接测试时,一共焊接了5块,其中有两块在有输入信号时无输出,其中焊
接的电阻电容的值和运放焊接都仔细检查过,都没有问题;实在是查找不到原因,仿真
时都是有输出的,因为我的滤波器焊接在中间级的,是否是由于我前一级的运放电路的
输出阻抗影响了滤波器的特性,导致200kHz的输入信号无法通过?具体原因还请帮我
分析一下;

有关OPA835的问题.pdf