采用PGA206标贴封装的放大器,但是当在VIN+引脚输入+5V直流电压,在VIN-输入GND时,为什么输出引脚与地间的电压只有3.2左右呢?引脚连接如下:1、2、3悬空4接地,5接+5V直流电压,6、7悬空,8接-15V,9悬空,10接地,11和12相连作为输出引脚,13接+15V,14接地,15、16为可控引脚。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用PGA206标贴封装的放大器,但是当在VIN+引脚输入+5V直流电压,在VIN-输入GND时,为什么输出引脚与地间的电压只有3.2左右呢?引脚连接如下:1、2、3悬空4接地,5接+5V直流电压,6、7悬空,8接-15V,9悬空,10接地,11和12相连作为输出引脚,13接+15V,14接地,15、16为可控引脚。
引脚9输出3.3V这点本身有问题了,为了快速定位问题,建议你换一颗芯片试试看
我用另一块板子进行了测试,发现还是有点问题,希望你们能给点建议。
供电正常(双极性供电),然后1脚输出是0V,9脚输出是5V,为什么输出只有4.1V呢?
如果我想调节输入offset votlage,在6和7脚接变阻器,变阻器的三个脚法是不是将可变的脚接到+15V,将满阻值的两脚分别接6和7即可呢?
从手册第8页图2来看,这样接是可以的,需注意的是变阻器的范围最好和图2中的相近。