最小能测量到的电流是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
IVC102的Data sheet中并没有给出确切的测量电流最小值,这个受积分误差的限制,受到input bias current等因素的影响,还需要考虑到对电路的增益,积分时间等要求。具体可以研读相关的Data sheet。
例如,IVC102的偏置电流最大0.75PA, 信号小于75PA,如不处理,误差>1%,信号为7.5PA时,误差10%。25度时,IVC102的失调电压最大5毫伏,55度时最大7.75毫伏,电流源电流与电流源内阻的积必须远大于7.75毫伏(至少100倍),否则引起误差.如0.01PA时要求内阻大于77.5万兆欧.