Other Parts Discussed in Thread: OPA847
求解:为什么运放输出端一般会串一个50欧姆电阻,然后又会接一个50欧姆的负载到下一级了?
如上图可不可以直接去掉R3,然后用R7进行阻抗匹配?另外R3的作用是什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
手册中有对此说明:
The Typical Characteristics help the designer pick a recommended RS versus capacitive load. The resulting frequency
response curves show a flat response for several selected
capacitive loads and recommended RS combinations. Parasitic capacitive loads greater than 2pF can begin to degrade
the performance of the OPA847. Long PCB traces, unmatched cables, and connections to multiple devices can
easily cause this value to be exceeded. Always consider this
effect carefully and add the recommended series resistor as
close as possible to the OPA847 output pin (see the Board
Layout section)
只有频率高到传输距离与波长相比拟时,才存在阻抗匹配的问题。另外如果是容性负载,输出端的电阻是为了抑制震荡