Other Parts Discussed in Thread: TAS5630, TAS5630B
敬爱的技术员:
您好!我使用的TAS5630!~~~AC220/35V输入的~~整流之后大概DC48-53V~
我想问问为什么多次开关机或使用2个月之后特别容易烧~大多数是开机烧的~
麻烦您尽快回复我好吗?
我想问问为什么多次开关机或使用2个月之后特别容易烧~大多数是开机烧的~
麻烦您尽快回复我好吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,这颗器件的建议供电电压PVDD_x Half-bridge supply, 为50V。
市电有20%的变化,如果市电变高后,整流后的结果超出芯片耐压啦。建议降低供电电压,或者供电采用稳压器后的电压。
开机的时候容易产生尖峰电压,建议软启动。
您好!工程师:
我用的是TAS5630B~耐压应该有69V的~
产生尖峰电压~应该是在继电器吸合之后是吗?但烧的时候继电器是还没有吸合的~开机大概5秒才吸合~但一开机不到0.1秒就看见火光了~芯片烧了~