Other Parts Discussed in Thread: OPA1632
如题,在使用OPA1632 时,我们把第7 引脚(使能引脚)直接接地了,请问这么连接正确吗,Datasheet 中未对该引脚的高低电平有效做明确说明
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OPA1632
如题,在使用OPA1632 时,我们把第7 引脚(使能引脚)直接接地了,请问这么连接正确吗,Datasheet 中未对该引脚的高低电平有效做明确说明
Datasheet 中有说明的:The shutdown (enable) function of the OPA1632 is referenced to the negative supply of the operational amplifier. A valid logic low (< 0.8V above negative supply) applied to the enable pin (pin 7) disables the amplifier output. Voltages applied to pin 7 that are greater than 2V above the negative supply place the amplifier output in an active state, and the device is enabled.
第7脚enble的电压为小于(V-)+0.8V时,运放输出被disable, 当大于(v-)+2V时,运放输出enable,按照你理解的意思其实相当于低电平有效。
您好,我想问一下,那运放使能要求电压是大于(V-)+2V的,您的意思是此时的电压是属于低电平。那么接一个上拉电阻接电源是否能满足使能的要求?
上拉电阻一般应该取多大呢?
EN使能引脚内部已经集成了50Kohm上拉,即使直接悬空,也保证了高电平,使得OPA1632一直处于使能状态。
有这个引脚是为了当有需要将其disable的时候,处于低功耗状态,降低功耗。