This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,请推荐工业0-5V输出集成芯片 谢!
0-5V输出集成芯片, 你应该详细描述一下功能要求
多谢提醒,是用在工业变送器上的,精度要求千分之一,稳定度要好,温漂要小些,用LM358运放搭的电路太占电路板面积
请参考RCV420这款工业应用,0~5V输出,4~20mA输入是否符合你的应用要求。
首先表示感谢,不过我想用单片机直接输出驱动0-5V,不想再增加一层4-20mA到0-5V的转换啦,那样会直接增加成本并影响精度及线性度的!
你已确定方案,那就用吧。注意通讯接口安全即可。
还没有方案,以前用LM358做的电路,精度不够好,希望推荐一下
你是希望弄个小个单电源精度较高的放大器对吧。看看这颗OPA313,单片机DA后给它放大即可。
应该是正解,谢谢啦!
你不考虑得到的0-5V的输出能力吗?没有什么要求吗?