This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA116测试100M高阻抗遇到的问题

Other Parts Discussed in Thread: INA116

如图1所示,利用INA116采集高阻抗负载,当电流源给电路通10nA的电流的时候,测得INA16的Vout端输出电压为1002mV(理论值1000mV),0.2%的测量误差,满足测量要求。

 图1

 

但是,当电路变成下图所示时,问题也随之而来了,如图2所示(在R1的下端再串联20M电阻R2)。同样的条件,电流源输出电流10nA,INA116的Vout输出电压变为1023mV(理论值1000mV);当降低电流源输出电流为1nA的时候,INA116的输出电压为121mV(理论值:100mV)。此时的结果已经是不可接受的了。即存在一个约20mV左右的误差?不知道是从哪里来的?感觉是交流干扰信号在20M电阻产生了电压(我们的系统是直流信号),感觉INA116已经是非常出色的一款仪放了,难道是INA116的CMRR低了?那也不至于这么大的误差吧。请TI工程师帮忙分析一下。非常感谢!

 图2