大家好,我们已经使用了TLV3801DSG一段时间了。在此基础上,后面我们会对电路进行一次改版,所以有些问题希望咨询TI工程师。
1. TI能否告知TLV3801DSG器件输入阻抗这个参数?我们在器件手册里似乎没有查找到这个参数。我们默认其输入阻抗很大,但是需要与TI确认。
2. 我们当前的前端电路示意简图,如下图所示。“比较器”即为TLV3801DSG,其输入信号来源于两级前置放大电路。现在为了简化电路,计划去除图中蓝圈中放大器。I-V转换前置放大器需要直接驱动比较器(TVL3801),I-V转换放大器电路的输出阻抗是100ohm~150ohm,输出信号上市时间很短(2~5ns左右),使用如此快速信号输入到TLV3801时,TLV3801DSG该如何对输入端口进行配置?是否需要进行50欧阻抗匹配,如果需要该如何实现?