This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV2771: 帮忙推荐一个适用于超声成像接收的前置放大器Amplifier选型和电路( recommend a preamplifier Amplifier for ultrasound imaging reception)

Part Number: TLV2771


TLV2771的带宽太小了,帮忙推荐一个适用于超声成像接收的前置放大器Amplifier选型和参考设计电路,需要工作带宽为0.5~20MHz,电压放大增益60dB,输入电容小于5pF。此外我还想问以下,我的输入端是压电晶体(频率几MHz),我需要的放大器设计有什么需要注意的吗,是必须要电荷放大器吗?

The bandwidth of the TLV2771 is too small, so I recommend a preamplifier Amplifier selection and reference design circuit suitable for ultrasonic imaging reception, which requires a working bandwidth of 0.5~20MHz, a voltage amplification gain of 60dB, and an input capacitance of less than 5pF. In addition, I would like to ask the following, my input is a piezoelectric crystal, is there anything I need to pay attention to in the amplifier design, is it necessary to charge the amplifier?