This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA240: 输出波形不正常

Part Number: INA240
Other Parts Discussed in Thread: LM311

你好,我使用ina240进行检流,电路原理图和pcb见图1和图2。被测电流是一个35k的正弦波电流。当两个参考电压都接地,输出波形反复横跳,如图3所示,理想波形应该是图4那样的仿真波形啊。当一个参考电压接电源,另一个参考电压接地,输出波形就是一个很好的正弦波了,但是总体被抬高vcc/2,说明芯片应该没有问题,请问为什么两个参考电压都接地,波形就不正常了呢。

  • 通过你的仿真波形,说明你输入的正弦电流信号直流偏置为0.

    电流放大器是单电源供电,

    负半周信号超出放大器共模输入范围。所以输出不可能正常。如果过大的话甚至可能损坏放大器。

    REF一个接5.0V,一个接GND,相当于给输出增加了2.5V的偏置。放大器可以工作正常。

  • “当一个参考电压接电源,另一个参考电压接地,输出波形就是一个很好的正弦波了,但是总体被抬高vcc/2“

    但并不建议这样使用,为保证精度,REF应该使用基准源提供

  • 我怎样才能得到关于0正负对称的放大波形,或者是不要负半周,得到就是像仿真波形一样的波形。另外你说的ref接到基准源,比如说2.5v的基准源,输出是不是就是被抬高到精密的2.5v?我其实是想把被测的正弦电流波形放大后,再变成高电平5v,低电平为0v的方波的,目前ref接到了vcc,输出波形被抬高到vcc/2,然后送入比较器lm311,lm311的阈值电压2.5v,我是通过电阻负压得到,由于被抬高的vcc/2不精确,比较器的电阻分压的2.5v也不精确,导致比较器的输出电平来回反转(当电流波形很小的时候,放大后的正弦波形也很小),这不是我想要的结果。所以我就想得到一个关于0正负对称的放大波形,然后比较器阈值电压设置为0,这样应该就不会导致比较器输出电平的来回反转

  • "所以我就想得到一个关于0正负对称的放大波形"对于INA240这样的单电源放大器来说,是无法输出小于0的的电压。

  • 如果你很希望使用INA240来处理这样的信号。建议后级增加一个双电源放大器。

    INA240的REF由REF3025提供,输出信号与REF3025差分,即可得到你说的关于0正负对称的放大波形。

    建议的方案是,不使用INA240。选择双电源供电的放大器,一级电路完成信号转换