This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Original question:
THS4524: CMRR 80dB, 可以加其他的方式提高吗?
想把四对差分信号放大100倍,这个器件可以吗?
您好,
不建议使用高于数据手册中的增益,
您也可以使用主页中提供的模型仿真测试您的电路设计,www.ti.com.cn/.../THS4524
那我需要放大100倍得话,是将两个放大十倍的ths4524级联可以吗?
理论上将两个放大十倍的THS4524级联起来,可以实现放大100倍的目标。但是在实际应用中,还需要考虑其他因素,如放大器的带宽、失真、噪声等。放大如此高的倍数可能会影响精度。