Other Parts Discussed in Thread: VCA810
专家们好,我做了一个VCA810的可控增益电路,但是调试的时候发现,当接入的控制电压为-1.5V时候输出出现了很大的毛刺,几乎自激了,整体的增益变化范围是-20dB到+20dB,请问该怎么调整使电路正常增益到-40到+40dB呢?期待着您的指导。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: VCA810
专家们好,我做了一个VCA810的可控增益电路,但是调试的时候发现,当接入的控制电压为-1.5V时候输出出现了很大的毛刺,几乎自激了,整体的增益变化范围是-20dB到+20dB,请问该怎么调整使电路正常增益到-40到+40dB呢?期待着您的指导。
下面是电路图和波形:
波形图是在控制电压为-1.6V,黄线是输入波形,绿色的是输出,这时候明显感到芯片发烫。请问各位专家这是为什么?我们该怎样怎么修改电路呢?另外我没有做PCB板,是在多孔板上连接的电路。谢谢。
专家们好,我做了一个VCA810的可控增益电路,但是调试的时候发现,当接入的控制电压为-1.5V时候输出出现了很大的毛刺,几乎自激了,整体的增益变化范围是-20dB到+20dB,请问该怎么调整使电路正常增益到-40到+40dB呢?期待着您的指导。
你好,你的这个现象是由于芯片出现了震荡. 在指标书的第22页, 有如下说明:
Socketing a high-speed part like the VCA810 is not
recommended. The additional lead length and pin-to-pin
capacitance introduced by the socket can create an
extremely troublesome parasitic network, which can make
it almost impossible to achieve a smooth, stable frequency
response. Best results are obtained by soldering the
VCA810 onto the board.
象这样的高速器件,建议你焊接在设计得当的PCB上测试.谢谢!