Part Number: THS4271
输入信号是连续载波(CW)或者是AM信号,频率在40MHZ,想要把信号放大到12V左右,自己设计了一个电路,但是放大倍数只有2.7左右,不知道是为什么。THS4271的增益带宽积是400MHZ,按理来讲40MHZ的信号可以放大十倍,但是实际运行时放大倍数远远不到,最多稳定在2.7倍左右。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THS4271
输入信号是连续载波(CW)或者是AM信号,频率在40MHZ,想要把信号放大到12V左右,自己设计了一个电路,但是放大倍数只有2.7左右,不知道是为什么。THS4271的增益带宽积是400MHZ,按理来讲40MHZ的信号可以放大十倍,但是实际运行时放大倍数远远不到,最多稳定在2.7倍左右。
您好,THS4271最大供电电压为10V没法满足您的设计需求,而且对于大信号输出12V 40MHZ,除了带宽还需要考虑压摆率的限制。建议您从下方器件中筛选。实际制板前建议仿真验证。