PACK+接到12V。负载用50欧姆水泥电阻。 测得R48两端电压0.9mV。放大倍数为100K/5K=20
用万用表测mV档R470两端电压,读数一直不稳定。从30mV持续增涨到200mV。
请问:
1、Vsense 为0.1mV,该期间能不能准确输出?
2、我们需要精确测试峰值40A电流,待机50mA,有没有推荐方案。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
PACK+接到12V。负载用50欧姆水泥电阻。 测得R48两端电压0.9mV。放大倍数为100K/5K=20
用万用表测mV档R470两端电压,读数一直不稳定。从30mV持续增涨到200mV。
请问:
1、Vsense 为0.1mV,该期间能不能准确输出?
2、我们需要精确测试峰值40A电流,待机50mA,有没有推荐方案。
1. 可以尝试INA212一类超高精度电流采样仪表放大器
2.电流检测的PCB布线需要使用开尔文连接方式
3.40A 和 50mA 分辨力要求不是很高,但是40A的电流 R48可能需要考虑散热问题,需要使用专门的检流电阻。
希望有回答你的问题