你好:
我用LM393输出驱动一个三极管8050来给一个外部设备传输脉冲信号,输出上拉电阻是4.7K到24V,
电源电压也是24V,现在输出经过三极管空载的话是标准24V脉冲输出,连接到外部接受设备,幅值马上变成了
14V左右了,外部设备是光耦接受信号,并且有个小LCD指示灯需要驱动,总起电流不是很大,为什么幅值会变化呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.