This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,OPA452(TO263-7)的散热部分和内部电路相连还是孤立的,如果是孤立的,是否可以接到电源参考点。如果和内部有连接,是连接到哪个管脚?
亲;散热器建议接到负电源。
如果采用正负电源供电也是连接到负电源吗;另外如果直流信号放大20倍,OPA452和OPA453哪个更适合一些,已经申请了OPA452是否可用?
亲,两者主要是高频特性不太一样,453单位增益积高些。30kHz以下信号放大时;两者基本没有区别。高于50kHz,453要好些。
如果正负电源供电,散热焊盘建议接在负压上,如果单电源供电的话,散热焊盘就和GND接一起。