Other Parts Discussed in Thread: OPA855,
我需要将一个nA,GHz级别的信号放大到mV量级,目前的做法是用LMH6629组成跨阻放大器作为第一级电路,OPA855组成比例放大器作为第二级电路,但是使用LTspice仿真后发现在10MHz到1GHz间电路的总均方根噪声达到了2.7mV,我需要将其降低到0.5mV,请问可能的改进建议。



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
针对您提到的在10MHz到1GHz频段内总均方根噪声达到2.7mV,并希望降低到0.5mV的需求,以下是一些可能的改进建议:
改进比例放大器(OPA855)的设计:
整体电路噪声分析:
请记住,每个改进措施都需要在仿真中进行验证,以确保它们不会引入新的问题或牺牲其他关键性能参数。