This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教:ISO124的单电源问题

Other Parts Discussed in Thread: ISO124, INA105

ISO124的单电源问题“

图1

   

图2

 

问题1:::根据官方的数据手册中图1,图2 电路是否可用,(1:+15V供电,15输入0~10V,2和3直接接地,)?
 图1中的IN4689 是稳压管吧,图2 就不用加了吧? 

问题2:::图1中左上角的供电电压与输入信号间的关系,当输入信号为-2~10V是,供电电压为20+V ??   

  • 1.你的图2想要表达的和图1有区别吗?图1的”-“也是连接GND.稳压管要加,它是将reference PIN控制在~5.1V

    2.是的,当然反过来说更准确

  • 1.我的意思是ISO124  15脚直接接信号输入, GND和-VS接地。稳压管是控制INA105的reference管脚,对后端的ISO124有影响吗??

    2.ISO124 供电范围:+-4.5V~+-18V,这里的20+V是什么意思呢??是指+VS相对于-VS的相对电压?

  • 1.如果你不要求GND PIN维持在5V的话当然可以拿掉

    2.就是+VS的大小,没有相对

  • 谢谢您的解答!

    1.这个参考电压有什么用?我今天搭面包板试了,当GND与-VS1接在一起接地时,输出不对,我给了GND一个+5V,-VS1接地,输出就对了,但是这样的话,我原来       1~10V的电压输入就变成- 4V~+5V的输出了。请教您一下这个GND参考电压具体是怎么用的?
    2.如下图:ISO124的供电要求均写的是+-18V,那这里又出来一个20+V是为什么呢??我今天用+24V做的,片子温度较高,能实际应用吗??

     

  • 回复神速啊,

    1.您的supply电压是多少?对应看看最上面你贴出来的那个表吧~

    2.看看这份名字的PDF文档:SBOA004,里面有提到For higher input range the circuit can be operated from a higher

    supply voltage.  SO---看起来是可以这么工作的,只是我觉得这个如果不需要的话还是别加那么大。 关于ABSOLUTE MAXMUN RATINGS里面的描述至少不算很冲突。

  • 我是想用24单电源供前端,+-15V供后端。现在由于GND引入了一个+5V,后边运放还得加法器去掉,就是不明白为什么非要加这个GND参考电压呢??

    SBOA004这个文档在哪?给个连接呗!谢谢!


    SBOA004这个文档  我找到了!!!!

  • hi,不准确的原因就看你输入的信号时多大和supply power是多大,而且上面给出的表格也只是在有5V参考状态下的,即如果你不需要5V,那你的输入就要相应的减去。