ISO124的单电源问题“
图1
图2
问题1:::根据官方的数据手册中图1,图2 电路是否可用,(1:+15V供电,15输入0~10V,2和3直接接地,)?
图1中的IN4689 是稳压管吧,图2 就不用加了吧?
问题2:::图1中左上角的供电电压与输入信号间的关系,当输入信号为-2~10V是,供电电压为20+V ??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.你的图2想要表达的和图1有区别吗?图1的”-“也是连接GND.稳压管要加,它是将reference PIN控制在~5.1V
2.是的,当然反过来说更准确
回复神速啊,
1.您的supply电压是多少?对应看看最上面你贴出来的那个表吧~
2.看看这份名字的PDF文档:SBOA004,里面有提到For higher input range the circuit can be operated from a higher
supply voltage. SO---看起来是可以这么工作的,只是我觉得这个如果不需要的话还是别加那么大。 关于ABSOLUTE MAXMUN RATINGS里面的描述至少不算很冲突。
hi,不准确的原因就看你输入的信号时多大和supply power是多大,而且上面给出的表格也只是在有5V参考状态下的,即如果你不需要5V,那你的输入就要相应的减去。