This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM386接上喇叭失真问题

如题,一产品使用LM386M-1,使用12V供电,测试如下:

1 在不接喇叭的时候,输出是OK的,波形也是比较好的正弦波(输入一正弦波测试),输出峰峰值为9.04V,如图片1所示

2 接上10R电阻(由于没有找到相应的电阻)测试,正弦波开始失真,顶和底部都有失真;输出的峰峰值为7.9V,如图片2所示

3 接上1W/8R的喇叭,输出就失真非常严重了,输出的峰峰值为5.04V,如图片3所示

原理图如图片4所示。

请问这是什么问题,需要如何解决?