This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lmp202x 搭建仪放输出问题

Other Parts Discussed in Thread: LMP2022, LMP2021

最近一直很郁闷,用一个LMP2022和一个LMP2021搭建了一个仪放,完全是按照数据手册上来的,用的是单电源3.3V供电,测试时发现当输入端压差为0零时,最终输出却不为零。Email咨询了TI的工程师,回复说单电源供电造成输入和输出共模范围受限的原因,让我在本论坛搜相关信息。我实在不理解啊,输入难道不在输入共模电压范围内?看数据手册上共模范围挺宽的啊。啰嗦了半天,马上上图,并且将仔细测试的结果也附上。

各点测试电压数据如下图,单位为V

从上面的数据可以看出,在输入小于5mV时,输出会有明显的失真,自己分析不了到底是前级的问题还是后级的问题。另外,我又做了如下3个实验,用lmp2022其中的一个运放做了3倍放大,以及做跟随器输出,其中一个跟随器在输出和输入Vin-端串了一20k电阻,当输入为0时,显然输出不为0,电路图如下

测试的各点电压数据分别对应下图中的3个表

实在是搞不定了,如何在输入为0时,输出也为0啊,并且能保证良好的放大增益,我的实际应用是对热电偶输出电压用仪放放大82倍,热电偶输出范围很小,只有0-8mV,跪求帮忙了。