为什么OPA357在输入0V时,用示波器测试输出时,有正弦波?
连接方式与datasheet第10页图2方式一样,RG=50Ω,Rf=240Ω,连接方式与datasheet第10页图2方式一样,RG=50Ω,Rf=240Ω,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,OPA357的数据手册中第10页没有图2,并且图2的原理图是Laser diode driver,并没有Rg和Rf的位号,麻烦再给一个准确的原理图和位号。
对于输入为0时,输出有正弦波,通常是出现了震荡,需要知道此测试的设计,如果有可能可以检查一下布板,这些都会照成不稳定的因素。
对于设计中的阻抗增益问题,你可以下载TINA的Spice库进行输出级仿真。地址为www.ti.com/.../opa357
建议可以先确定输出正弦波的频率,然后可以通过简单方法确定振荡频率源。
我们可以看到OPA357是CMOS运放,因此其等效输出端会存在一个等效电容值,而简单的电阻反馈是不会影响其相位和闭环增益曲线的斜率的,如果在输入端没有问题的话,我们可以推测在输出端存在一个等效阻抗(Ro与某一未知阻抗)与等效电容共同作用影响了运放环路的稳定性。
当然通过PSPICE可以完成系统稳定性仿真,那就是主要通过观察其输出闭环增益,与对应的相位曲线来判断其稳定性。
如果想查看CMOS运放的等效模型可以参见Tim Green的运放稳定性(7),上面对CMOS模型有解说。
希望能回答你的问题!