This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
正负5伏供电
亲;热到啥程度?散热垫是如何处理的?
用手摸着烫,芯片也不工作,输出是3.8伏的直流信号;我的PCB是这样的
散热方面没做啥处理
亲;这种放大器,需要将电源退耦和反馈都装IC跟前,远了非常容易自激。建议用示波器观察一下输入输出。
试过单电源0到5伏供电,示波器上显示的是直流
亲;如果有些烫手,是正常的。
这颗料的静态电流大约27mA;+-5V时的静态功耗为0.27W。你的这种用法热阻大体在135C/W,温升为36C。夏天;实验室温度大多在25~32C,那么;IC实际表面温度会在61~68C。
你能忍受不撒手的温度;大体在60C水平!所以;“烫”在夏天,一点也不奇怪。
你可以用IC上的那个散热垫焊到PCB覆铜上;用铜皮散热,对于1盎司厚铜;1平方英寸的热阻大体在83C/W。这样;IC温升会降到22C,就不会那么烫了。
你好,检查下电路先,退偶要尽量靠近电源引脚处理,信号引脚走线太长很不适合这种高速运放。