This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA862: 单端转差分运放选型咨询

Part Number: OPA862

您好,我现在有个差分输入的ADC(单片机MKM35Z512VLL7内部的AFE模块),接受峰峰值1v的差分信号输入。如下图数据手册截图所示:

        我需要一款运放能把我现场传感器的单端信号转为差分输入给ADC。

        之前我用的是全差分运放,使用REF35120QDBVR加电阻分压、运放跟随的方式,产生了一个0.6V的电压。设置全差分运放的Vocm为0.6V,打样后全差分运放工作不正常,后来看数据手册发现Vocm的值是有要求的,单电源供电的情况下,Vocm>0.8V才能正常工作。

        现在我的样板,运放供电是单电源5V,运放封装是8-Lead SOIC,Vocm是0.6V。我打算换个运放接着实现我的功能,我在ti的选型手册里找到了OPA862这款运放,但我没找到他对Vocm的要求,是因为他不是全差分运放所以没有这个要求么?他能支持0.6V的Vocm么?

        还有我想请教一下,运放模拟一般用什么软件?我是用LTspice仿真时,软件并没有提示我Vocm取值不正确。