您好,我的应用是OPA124UA的供电离放大器比较远,大概会有0.2V的压降。供电侧电压为正负5V,这样OPA124UA的管脚电压只有正负4.8V了,这个电压会对OPA124UA造成多大的影响,是性能上的还是可靠性和寿命上的?我无法把电压端调高,因为近端用了CD74HC4351,他的供电最大只能正负5V,请问正负4.8V的电压有问题吗,或者有没有可替换的放大器(低功耗)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我的应用是OPA124UA的供电离放大器比较远,大概会有0.2V的压降。供电侧电压为正负5V,这样OPA124UA的管脚电压只有正负4.8V了,这个电压会对OPA124UA造成多大的影响,是性能上的还是可靠性和寿命上的?我无法把电压端调高,因为近端用了CD74HC4351,他的供电最大只能正负5V,请问正负4.8V的电压有问题吗,或者有没有可替换的放大器(低功耗)
OPA124最低工作电压为+-5V,为了保证长时间的性能,不建议低于这个电压范围使用。可以看看OPA137,OPA234,OPA131等。
感谢推荐
我的应用中,运放的前端是高阻,所以我的理解是需要电流噪声很低,输入阻抗很高(GΩ级)的运算放大器。我的应用对噪声的要求很高。我原先选择的是另一家的AD795JR,后来看到OPA124UA在噪声上要比AD795更好,只是功耗略高一点但可以接受。通过仿真和测试也证实了这一点。但由于供电的原因,我一直觉得不保险,所以希望各位大侠能帮忙给点建议。GBW在1.5MHz就够了,若再低,我就需要提高后级增益,噪声也会提高。
上面提供的几颗放大器好像都无法满足我的要求,烦请各位大侠再帮我看看,感激不尽
如果是这样的,确实不好找。你看看OPA121吧,它的供电范围宽一点,带宽也能满足,输入阻抗也比较高,噪声是6nV/ÖHz, 10khz,偏置电流是5pA比opa124稍大
我还有一个思路,就是把电源设置到±5.2V,通过长线缆传过去正好是±5V左右,然后近端的多路复用器的电源上能否串一个电阻来降到±5V或±4.5V给多路复用器用,如果这种方法可行,那么用多大的串阻降压合适呢,谢谢
然后OPA121的供电最低好像也是±5V
POWER SUPPLY
Rated Voltage ±15 ±15 VDC
Voltage Range,
Derated Performance ±5 ±18 ±5 ±18 VDC
Current, Quiescent IO = 0mADC 2.5 4 2.5 4.5 mA
由于运放消耗的电流不是固定的,那么电缆线引起的压降也不可能一直是0.2V,你可以再提升一下供电电压。
根据多路复用器的电流消耗情况确定串多大电阻吧